5/25/2010 5:14 PM | |
Joined: 9/27/2006 Last visit: 1/19/2025 Posts: 12330 Rating:
|
Hello Abyrne: To start with, here is some general information on the ET 200S: https://www.automation.siemens.com/mcms/distributed-io/en/ip20-systems/et200s/Pages/Default.aspx?HTTPS=REDIR Look further here for specific info on the CPU Im 151-7, and the Modbus/USS serial module 1SI (with dowloads of dedicated function blocks for the 1SI): : Manual for ET 200S serial modules: http://support.automation.siemens.com/WW/view/en/9260793 Sample programs for the 1SI Modbus serial module: http://support.automation.siemens.com/WW/view/en/25358470 ET 200S IM 151-7 CPU manual: http://support.automation.siemens.com/WW/view/en/12714722 Look up the stats on the IM 151-7 CPU in thelast manual, as far as I/O count and selectable modules. There is also a list of ET 200S manuals shown, so you can locate more information as you need it. |
Last edited by: dchartier at: 5/25/2010 7:05 PMAdded link to ET 200S portal webpage. Last edited by: dchartier at: 5/25/2010 7:03 PMLast edited by: dchartier at: 5/25/2010 5:16 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on