6/10/2010 2:46 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, First of all - did you check if PC card is healthy? Let's say with connection to other device or internet. Is this IM151-8 CPU a new one or existing (working) in field? You could find good explanation how to connect programming device to the IM151-8 CPU in SIMATIC ET 200S distributed I/O IM 151-8 PN/DP CPU interface module manual. (Chapters PG Communication and Connecting a programming device / PC to the integrated PROFINET interface of the IM 151‑8 PN/DP CPU interface module... Best regards, Hristo Mihalev |