5/20/2014 7:56 PM | |
Posts: 17 Rating:
|
Hello, I have a system with one im151-8 cpu (6ES7 151-8AB01-9AB0) and few ET200S IO (6ES7 151-3AA23-0AB0). I've configured MRP topology, assigned partners for each port. I've assigned roles for im151-8 as manager and 151-3 as clients. Everything is ok. But when I turn off one of the et200s im, I lost half of the et200s im, connected between second port of im151-8 cpu and break of the ring. It looks like only one port of the im151-8 can connect 151-3 and ring doesn't work. Why does it happen? What did I wrong? I've attached pictures with topology editor online when everything is ok and when one of the 151-3 was turned off. Attachmentpic.zip (74 Downloads) |
Last edited by: AndreyCh at: 5/20/2014 8:42 PM |
|
Follow us on