10/23/2017 10:59 AM | |
Joined: 4/8/2009 Last visit: 3/19/2025 Posts: 83 Rating:
|
Hello Everyone, We are facing communication loss problem between PLC-S7-400H and RIO Panel. This RIO Panel having two ET200M Rack communicating with PLC on profibus. IM 153-2 Redundancy bundle is used in ET200M Rack. Profibus OLM is used in RIO panel to convert fiber optic to Profibus. one ET200M (profibus address 7) is communicating with PLC without any problem. Another ET200M (Profibus address 6) having frequent communication loss problem with PLC. Once communication loss between profibus node 6 and PLC, after few seconds same node automatically communicates again with PLC. This communication loss happen frequently in night time only. In day time only 2 to 3 times happen. Please find attached screen shots for CPU diagnostic buffer and Profibus Network diagram. Please advice on this.
Thank you AttachmentDignostics.zip (131 Downloads) |
Follow us on