12/29/2014 12:31 PM | |
Posts: 8 Rating: (0) |
we have same problem with IM154-8FX PLC when using the motor starters. we have about 10 control system with hardware as well as software configurations. out of this 5 system has 5 system gots the problem "PROFINET IO module removed/cannot be addressed" for slot number 11 consistensly for all. for other 5 system it for slot no.12. the fault gets automatically reset in few miliseconds. below are the diagostic buffer history. Event 1 of 10: Event ID 16# 3854
pls suggest the remedy. Chetansing Patil ------- New subject after splitting from Module/Interface Module removed/cannot be addressed. |
Last edited by: Min_Moderator at: 12/29/2014 1:50 PMSplitted |
|
12/29/2014 1:51 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on