2/26/2014 3:23 PM | |
Joined: 6/24/2013 Last visit: 10/7/2024 Posts: 1628 Rating: (421) |
for standard panel pc running windows you can use http://www.backup-utility.com/download.html click local download to gewt it 1. it is free of charge for both home and business use!!! 2. it can create image of the whole system and compress it 3. creates the bootable stick [16gb stick should be enough to store bootable part and panel pc backup as well - backup is compressed] 4. it can mount image as a virtual drive so one can get some data from it instead of restoring whole hard drive this may help and is FREE Tested/working on Amplicon panel PC running SCADA |
3/4/2014 3:14 AM | |
Posts: 1 Rating: (0) |
After purchasing the image creator SDK, you will get the license key to activate the imaging SDK and use controls included in it to create, convert, annotate and process your images. |
Follow us on