8/11/2017 3:09 PM | |
Posts: 19 Rating:
|
Dear Experts, I have small issue I have emf graphics files which I import to TiaPortal WinCC V14 SP1 UPD1 and after import TIA is changing size of this graphics from 43x43 to 27 x 39. Is there any option which will allow me to keep source size. Later I can show this graphics and adjust size to 43x43 but it is already deformated. I want to have graphics with option "Fit object size to graphic" In attachments example graphic which I am importing.Checked also with MS Word and it is importing also wrong size. Any ideas why? BR, Lukasz AttachmentCentrifugal Pump D [activated].zip (44 Downloads) |
Last edited by: ld22 at: 8/11/2017 3:22:35 PM |
|
Follow us on