Industry Online Support
Technical Forum
11/19/2008 11:48 AM | |
Posts: 31 Rating: (0) |
Hello everybody! In my work im using now Simotion C230 and Simodrive 611 universel and i need to feed KL 663 (Impulsfreigabe baugruppenspezif) and KL 65.x (Reglerfreigabe achsspezifisch) on Simodrives powermodul. But i dont want to make another switch on test bench with wich im working. So im trying to do it with SIMOTION.Signal from enige`s sensor goes on converter and from convertor modified signal goes on SIMOTIONs interface X4. Soim using X4. It mean that it is axis 2. But it seems like im doing smth wrong while parametrizing axis 2, cause it comes mistakes connected with adressation. In attachment there are examples of my program and mistakes that i have. Could anybody help me with this please? Best regards, Tanya AttachmentSim_doc.zip (360 Downloads) |
11/24/2008 12:57 PM | |
Posts: 4 Rating: (0) |
Thank you very much for your as usual helpful answer) |