8/11/2016 8:48 AM | |
Posts: 4 Rating: (0) |
i have some problem.. I have a S7 319CPU with a profinet connection to a et200s module (153IM).i have 20 pieces et200s module on the hardware. i use Step7 V5.5. Via the menu PLC ==> Edit Ethernet node==> Assign device name but In the HW Config i cant see one et200s module.the others ok.. I replace it with a new one but i cant see module. I was given a new name and ip adress but i cant see module. please help...thansk ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/11/2016 10:25:05 AMNew subject after splitting |
|