8/29/2008 7:52 PM | |
Posts: 3 Rating:
|
|
8/29/2008 8:28 PM | |
Posts: 3 Rating:
|
When using the BT200 i amgetting a cablelength distance more then twice of the reflective distance.I am seeing the condition on 40% of the 60 systemsI tested.When doing repeated test on the same system sometimes it works OK. i checked connections repeatedly without any good results.We are using Turck interfaces. also used Step 7 Topology test to confirm lenght. Any thoughts. Glen attached is BT200 test results with repeated cablelength test. AttachmentOP40-9 RE-TEST 8-26-08 BT200.pdf (348 Downloads) |
9/2/2008 3:11 PM | |
Posts: 5822 Rating:
|
Dear GMB, have you tried to figure out if the reflection test worked out with your Cable segment yet? Best regards J_Bell |
Follow us on