11/12/2018 5:38 AM | |
Posts: 171 Rating:
|
We're using 1518-F CPU and it is running out of retain memory ( 700KB ). Showing 100 % usage in program info. 6ES7518-4FP00-0AB0 Is there any possible way to increase this memory. I think there is no way to do this. But am asking whether its having any solution. We're working on a standard in which one protected DB itself having size 450KB. |
11/15/2018 5:42 PM | |
Joined: 7/7/2010 Last visit: 9/29/2023 Posts: 13751 Rating:
|
You have that much data that changes after startup that isn't dynamically recalculated? This is maybe a case for an external SQL server or external computer where recipe or process data is stored. I guess what I am saying do you really have a large amount of truly independent data to store, or a large amount of data that could be determined at recipe change / startup, but nobody wants to do that?
|
science guy |
|
This contribution was helpful to
2 thankful Users |
11/16/2018 7:45 AM | |
Posts: 171 Rating:
|
thankyou for the reply...no recipe is used.. now the problem is solved by deleting some unwanted tags. |
Follow us on