Industry Online Support
Technical Forum
6/7/2007 8:35 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating:
|
Hi, I have some links for you, so you can download some handbooks. Linksto free offline Webbased managers: Free Offline Version for Demonstration Purposes of the SCALANCE W788-2PRO Web Interface Free Offline Version of the SCALANCE W788-2RR Web-Interface for Demonstration Purposes Free Offline Version of the Web Interface of SCALANCE X-200 and SCALANCE X-200 IRT Linksto the Wireless manuals: SCALANCE W788-1PRO (Access Point) SCALANCE W788-2PRO (Dual Access Point) SCALANCE W744-1PRO (Ethernet Client Module), SCALANCE W746-1PRO (Ethernet Client Module), SCALANCE W747-1RR (Ethernet Client Module IPCF) Gateway IWLAN/PB Link PN IO for Industrial Ethernet / Manual Part BL2: Linksto Wireless Accesoires: RCoax System Manual Update RCoax: ANT793-8DR (Directional Antenna 5 GHz) (20 degrees) ANT795-4MR (Omni Antenna 2.4 / 5.25 / 5.8 GHz) (Standard diversity antenne's) ANT795-6MR (Omni Antenna 2.4 / 5.2 GHz) ANT792-8DR (Directional Antenna 2,4 GHz) (30 degrees) IWLAN Antenna extension cable FRNC Linkto manuals Industrial Ethernet switches: SIMATIC NET Operating Instructions Industrial Ethernet Switches SCALANCE X-400: http://support.automation.siemens.com/WW/view/en/19625216 SIMATIC NET Configuration Manual Industrial Ethernet Switches SCALANCE X-400: http://support.automation.siemens.com/WW/view/en/19625108 Industrial Ethernet SCALANCE X-100 and SCALANCE X-200 Product Line: http://support.automation.siemens.com/WW/view/en/22305980 Industrial Ethernet SCALANCE X005: Linkto ethernet accesoires: Industrial Ethernet SCALANCE X-100 Media Converter If you want more, then you may find it on the page. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
6/7/2007 9:53 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Zuhluf, In addition to the links Late allready placed in this topic I want to mention the following links: GPRS/GSM-Modem SINAUT MD740-1 System manual: http://support.automation.siemens.com/WW/view/en/23940893 Basics of Industrial Wireless LAN http://support.automation.siemens.com/WW/view/en/9975764 And then a very important but large manual. Communication with SIMATIC http://support.automation.siemens.com/WW/view/en/25074283 Good luck reading it. |
Best regards, |
|
Follow us on