8/16/2019 7:31 PM | |
Posts: 20 Rating:
|
Dear, i am planning to upgrade ASRS cranes with S120 drive system warehouse is powered by National Grid Line in Northern Ireland, we are using 1 step-down transformer for whole SITE, means 400V line will be common for all cranes, where as each crane will have independent panel with VSM10+Basic Line Filter+AIM+ALM+MoMoeach crane have 3 motors= 18.5KW+15KW+0.55KW, basic power sketch is attached if i use SLM how much PF can be affected / get poor as compare to use of ALM i have also attached the part #s of items i have selected to achieve below benefits of ALM 1-stable DC voltage 2-approx. harmonics free current 3-reuse of regenerated energy please confirm all selected items are OK? i have already used BLM & ALM previously but with simple application AttachmentALM Config.zip (32 Downloads) |
Follow us on