7/15/2024 10:21 AM | |
Joined: 1/21/2013 Last visit: 10/12/2024 Posts: 3174 Rating: (491)
|
Hi Scyzoryk96, A more detailed description would help us understand your problem. What I understand is that you have done some scripting on the OnActivated event of an IO field that no longer fires when you click on the IO field. I have not observed this behavior in PC Runtime V19 Update 2 (I have not jetted the Update 2 SR1 from last Friday). And also not on a MTP1200 with the current image version V19.0.0.2. The changes to get a fix if there is a bug will increase dramatically at the moment as development gets knowledge of the problem. To make sure they know, you should create a support request. Kind regards |
Follow us on