12/1/2023 1:33 PM | |
Joined: 12/15/2015 Last visit: 1/24/2025 Posts: 6 Rating: (0) |
Hello. Its nice. Can be used if IO is on screen. But I have IO in faceplate and this event is not avaiable.... Actually im in struggle, because Im moving value from HMI tag which is connected to PLC to HMI UDT, which is Internal tag. When I enter value in Faceplate I like to update oposite way. But without this event its hard. Still not figured out the solution with uncheck Accept value after exit... Good God Siemens. Do the job properly ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/04/2023 05:08:26New subject after splitting |
|
Follow us on