10/11/2018 12:09 PM | |
Joined: 2/12/2018 Last visit: 11/26/2024 Posts: 224 Rating:
|
Hello my good people I am using a CPU1513, TP1200 Comfort, TIA15 and WinCC Advanced. I have made a remote access to my HMI by using Sm@rtServer/Client. It is working like it should both in the Sm@rtClient program and in a internet browser. My problem is that you can only use one screen at a time, either the HMI or the PC with Sm@rtClient. Whenever I am using one of them, the other one gets a 'No input' (see attached picture) whenever you press on something. Probably to prevent someone to eg. use the HMI, when another is using the PC. But I dont know how to get out of it. If I have used the PC, and now will use the HMI, I need to click on the screen many times before the 'No input' goes away and I can use the screen. And it is the same the other way around. So my question is, do anyone know how to get away from 'No input', when you go from one device to another? Best regards |
Please don't forget to rate :) |
|
Follow us on