9/19/2010 5:59 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hi what is the maximum frequency of input signal of the FM351-1 .As I checked in the manual the max voltage suitable for this is 24 volt.What should be done for higher signal levels. Best regards Attachmentfinal.zip (252 Downloads) |
9/19/2010 8:46 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating: (11) |
Hosseini, Downloadthe manual for FM351 from this following link: http://support.automation.siemens.com/WW/view/en/2103043 Check outAppendix A - Technical Specification - Page 160. Regards, Behnam www.sigmaprocess.ca |
9/19/2010 8:50 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating: (11) |
Hosseini, How high is the voltage and what is the frequency? Regards, Behnam www.sigmaproess.ca |
9/7/2017 3:20 PM | |
Joined: 8/21/2014 Last visit: 9/17/2024 Posts: 1024 Rating: (14) |
New question published by AutoGen_148962 is split to a separate thread with the subject Connection SSI signal output of a LVDT to FM351. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on