12/7/2018 1:37 AM | |
Posts: 1 Rating: (0) |
It is interesting to note that the "6ES7 511-1AK02-0AB0" datasheet indicates that it is possible to configure with older versions of TIA portal: "V15.1 (FW V2.6) / V15 (FW V2.5) or higher; with older TIA Portal versions configurable as 6ES7511-1AK01-0AB0" I could do a hardware download to Using TIA V13 SP1 and the LCD panel on the front would inciated "TIA V13 SP1" and Firmware "2.5". But inside the TIA program it would indicate as a "6ES7511-1AK01-0AB0" with Firmware Version 1.8. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/7/2018 10:37:14 AMNew subject after splitting |
|