1/9/2008 3:22 PM | |
Joined: 1/7/2006 Last visit: 2/16/2023 Posts: 2705 Rating:
|
Hi, Which version do you have, have you looked on the first page of this thread, that are the versions that are given free and also works. (thread is splitted, first page of thread: VISTA Ultimate with STEP7) |
Last edited by: Late at: 11.01.2008 22:55first page mentioned of the right thread I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/10/2008 8:25 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating:
|
Hi, In the link http://support.automation.siemens.com/WW/view/en/26578452is also mentioned that you have to install SP3 first, then you can install SP3.1. The other softwarepartsof STEP7 Professional have to be downloaded and installed separately. Therefore the link Spät provides us are very useful. |
Smurf |
|
3/14/2008 3:49 PM | |
Posts: 1 Rating:
|
I am having simular problems... I have set the compatibilitymode of the installer to "xp service pack2", but I can't seem to install it on vista itself... |
Follow us on