10/17/2011 9:48 AM | |
Posts: 270 Rating: (53) |
Hello Zee.Alam, have you checked i.e. this post, where the problem has been discussed before? It should help. /tf/WW/en/Posts/57764 |
10/17/2011 10:52 AM | |
Posts: 270 Rating: (53) |
Yeah, obviously they were talking about need for flexible 2008 sp2, flexible 2008 no sp or sp1 are NOT COMPATIBLE with windows 7 (http://support.automation.siemens.com/WW/view/en/22055368). That's why you need to get that installation CD with SP2 included as it is suggested in the thread i linked. EDIT: Also this might be helpful to add: https://www.automation.siemens.com/tf/WW/en/Posts/24698 |
Last edited by: MM1234 at: 10/17/2011 10:56 AMGah, no can do links in the edit notes :( Last edited by: MM1234 at: 10/17/2011 10:55 AMAlso this might be helpful to add: /tf/WW/en/Posts/24698 |
|