3/28/2022 7:19 PM | |
Joined: 8/4/2021 Last visit: 1/18/2023 Posts: 7 Rating:
|
Hello, I have followed Der Hecht video about installing Node RED with docker and industrial publisher. I use MTP700 Unified panel and TIA V17 I did instal the app I can see it in EDGE (browser), but I cant open NodeRed I have warning that "APP is not running" I downloaded the LOGS and there is error: Error: EACCES: permission denied, copyfile'/usr/src/node-red/node_modules/node-red/settings.js'->'/data/settings.js' Dont U pls know what to do ?? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/29/2022 09:41:26New subject after splitting |
|
3/31/2022 11:17 PM | |
Joined: 9/21/2006 Last visit: 1/27/2023 Posts: 241 Rating:
|
Make sure that you have the latest version of the Node-red dockerfile from Industrial Edge applications in conjunction with the SIMATIC HMI Unified Comfort Panel. There have been several tweaks to the configuration over the last year, including changes to the CMD line that tells node-red where to find its settings.js file. Use the docker-compose.yml file that comes in the application example as the starting point in IEAP - it sets up data mappings and restart options that if set wrong, can stop the app from running. |
Follow us on