4/21/2015 6:11 PM | |
Posts: 33 Rating: (0) |
Hi guys, Today I installed TIA WinCC v13 SP1 (all the updates included). After installation I got: Software licensed :Simatic HMI -WinCC Professional -see attached .So far so good Since I'm still excepting the hardware to come , I wanted to simulate a project I've already developed .First thing I noticed was that the Runtime button was disabled , so I couldn't use it.Don't know why! Anyway ,I've used the 'Start Simulation' command using the mouse .After a few seconds , the runtime session displayed a message saying'Too many tags(powertags) have been configured.WinCC Runtime Advanced 128 Powertags v13'. Which is strange because: 1- I've sign up for a Professional Runtime license(512 powertags) , and not an Advanced Runtime with 128 power tags. Below is the product description I bought and installed: https://mall.industry.siemens.com/mall/en/uk/Catalog/Product/6AV2103-0DA03-0AA5 2-I've checked and I'm using only 22 power tags (process tags);less than 128 power tags anyway . What I did next , I verified if the Professional Runtime license(512 power tags) was installed and it wasn't and neither the advanced runtime license!-see attached . And this might explain why I got this message . Now , since the item I bought (6AV2103-0DA03-0AA5) says it has included Advanced Runtime and Professional Runtime(512 power tags) Licenses , why the I can't see them as being licensed . During WinCC v13 SP1 I haven't got any error messages .Please see the attached pics . Thanks aney_312
AttachmentInstallation Pics.zip (197 Downloads) |
Last edited by: aney_312 at: 4/21/2015 6:15:49 PM |
|
4/22/2015 12:02 PM | |
Posts: 33 Rating: (0) |
Hi Cristoph, That's a good thing to know. I presume that when I'll be online with TP1200 the message will disappear . Regards aney_312 |
Follow us on