Industry Online Support
Technical Forum
9/12/2012 9:35 AM | |
Joined: 7/8/2012 Last visit: 3/24/2022 Posts: 13 Rating: (0) |
Hi, I have a problem with my INSYS GSM. it is not talking with my LOGO. I tried number of ways. When i given an alarm input to INSYS it is given the replay, but when i connected with Logo and run the program the Insys not responding. RX/TX is not flashing. I tried the way that i given a "STATUS?" sms to INSYS then that RX/TX LED is just blinked and Status LED is blinked three times. But i didnt get any response back.. I have checked the history in that it is showing 'GSM ERROR'. My LOGO Part number : 6ED1 052-1FB00-0BA0 My LOGO PC Cable part No : 6ED1 057-1AA00-0BA0 Please check the attached Insys settings also. AttachmentInsys.zip (208 Downloads) |
Last edited by: O_Moderator at: 9/14/2012 10:06 AMnew subject after splitting from /tf/WW/en/Posts/5506#top |
|
10/8/2012 4:42 PM | |
Posts: 378 Rating: (73) |
Hi Midhun Pius, 1. It seems you didn't load PLC data ( .gsp file), Request INSYS for LOGO data or you can find on your CD then load to your configuration by> HSComm GSM> PLC > Load PLC Data. 2. I have a doubt weather your LOGO OBA0 is compatible with your INSYS GSM re-confirm with the manufacturer. Regards |
Follow us on