1/18/2010 9:50 AM | |
Posts: 1 Rating:
|
Hallo, i try to connect two PLC's over the integrated communication device. One is a 317F-2PN-DP (FW 3.1) and the other is the 319F-3PN-DP (FW 2.6.5). I used the example of Siemens to connect both and this seems to work, but when I try to send/receive datas there comes an error. Sender error 8092 Empfänger error 897f The Connection was created by the OC-Wizard and than I make the last changes in the FB460 by myself. In a first step I had to change the SFC20 to the SFC83, because there was an error W#16#8092, so I changed. Has someone an idea what the problem is with the sending error? In the zip file is the whole project. Thanks for everyone who can help me. Benedikt AttachmentEthernet.zip (85 Downloads) |
Follow us on