11/23/2006 3:32 PM | |
Posts: 3149 Rating:
|
Hi, well, I´ve not heard of such problems...but I guess that after deinstalling/installing WinCC flexible again, everything should work. nemo |
11/24/2006 7:02 AM | |
Joined: 12/12/2005 Last visit: 3/18/2023 Posts: 178 Rating:
|
[8)]So I´m first one[8)] Nothing wrong in programs[:D] /tf/WW/en/Posts/5282 Maybe I ´m only one (***) or doing something else wrong but this is real problem, and I have to solve it. No, ofcource I triedinstall programs again butit not help.Step7 working but integration not anymore. WinCCflexible need RAM over 1GB, I had 512Mb and I raised it to 2Gb but no effect. Also big problems transfer winccflex. program to panel??? Hessu |
Last edited by: Heksu at: 11/24/2006 7:11 AMLast edited by: Heksu at: 11/24/2006 7:09 AM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
11/24/2006 8:45 PM | |
Posts: 3149 Rating:
|
Hi, which other software is installed on your system? Did you install first STEP7 and then WinCC flexible? Do you have the same problem on other PCs? nemo |
Follow us on