11/22/2021 3:17 PM | |
Joined: 9/27/2006 Last visit: 7/8/2025 Posts: 12373 Rating:
|
Hello Gajendrad.s; The IM 155-6 ST is an interface module for ET 200SP remote I/O systems. Tere is no problem connecting ET 2000SP modules to a S7-1200 CPU, over Profinet. See this quote from ChristophD, and examine the posts by others in the link below: "Remote I/O is not depended on the PLC Type. You can use the Distributed I/O from ET200S,Et200M, ET200SP, ET200MP with the S7-1200." https://support.industry.siemens.com/tf/ww/en/posts/s7-1200-remote-i-o/142543 Hope this helps, |
11/22/2021 3:35 PM | |
Joined: 8/9/2011 Last visit: 5/27/2025 Posts: 324 Rating:
|
Hi, Thank you for your response. i want to confirm i dont have only s7 1200 CPU. It has many DI, DO, AI modules already as expansion. My query is- is it allowed to use these IO modules along with interface modules? |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
11/23/2021 6:05 AM | |
Joined: 5/12/2006 Last visit: 7/7/2025 Posts: 22661 Rating:
|
yes is possible. |
12/6/2021 12:02 PM | |
Joined: 9/27/2006 Last visit: 7/8/2025 Posts: 12373 Rating:
|
Hello GajendraDS; Good to know you have found a solution to this problem. The "address" shown in your first image above (12/6/2022) is the MAC address of your IM 155-6. A unique MAC address attributed to all Ethernet modules in service in the world today, as a way to distinguish them. That is why Etherney modules all over the world can use similar IP addresses on their own network, without confusion, the MAC address is unique. If the IM mosule loses its configured IP address and PN name, it reverts to its MAC address, ss your screenshot shoeed. See if the information contained in this document can clarify the issue, if it ever happens again: it also shows that you can use a Bus Adapter server module on each IM 155-6 to maintain the IP address and Profinet name of the IM in case of power loss for example. https://support.industry.siemens.com/cs/us/en/view/36752540 Hope this helps, |
Last edited by: dchartier at: 12/06/2021 12:06:13Last edited by: dchartier at: 12/06/2021 12:09:03 |
|
Follow us on