5/24/2018 10:29 AM | |
Posts: 3 Rating:
|
Hello Experts, We use a crane with s7-300 having 3 stations connected remotely and controls 4 drives. We are unable to figure out the reason for a communication loss between the stations which occurs only when the hoist is brought down. The system trips with the diagnostic buffer attached in the post. The HMI shows overweight and over-speed signals during the fault. This is consistent with loss of signals from one of the PLC racks(no:23) since over-speed and overweight are NC contacts which trip in case of fault. We have done the following already 1. Exchanged the PLC racks with already working cranes. 2.Exchanged/verified all sensors connected with the system concerning hoist working. 3. Checked all connectors in the PB connectors for shielding and short circuit 4.Routed an external wiring for the network to eliminate harmonics. There have been no improvements in the system till now. Kindly suggest possible solutions from experiences which you have had in the past. Also please suggest if I am missing something. AttachmentDiagnose.txt (108 Downloads) |
Follow us on