7/11/2019 9:34 AM | |
Posts: 153 Rating: (7) |
Hello PISCEAN, Can you tell me when internal EMF used which of these parameter are active: 1. Rated Speed parameter p50119 2. EMF rated ValueP50118 3. Speed Controller EMF at Max Speed P50115. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/11/2019 13:25:24New subject after splitting |
|
7/11/2019 1:29 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (878) |
If p50083 = 3, then specifing EMF max speed p50115 is to be set so that speed is adjusted using EMF as speed actual value. HTH |
This contribution was helpful to1 thankful Users |
Follow us on