4/2/2008 4:57 PM | |
Posts: 2661 Rating: (279) |
The first thing I would try is, to save-as the project with reorganization and a different project name. Please note that changing the name of the project when you save-as is absolutely vital since some types of project corruptions do not get "cured" if you save-as with the same name and just a different folder. Also see the following FAQ: Why does the message "S7tgtopx.exe has caused an error and will be closed" appear? http://support.automation.siemens.com/WW/view/en/13770987 |
This contribution was helpful to1 thankful Users |
4/3/2008 3:35 PM | |
Posts: 23 Rating: (0) |
Did you open your project in a different version of the programm (5.3/5.4). I had the same note after I've done that, but it was working |