4/8/2015 7:43 PM | |
Joined: 3/28/2015 Last visit: 11/7/2024 Posts: 721 Rating: (213) |
Kindly find the attached file. P0640 Defines motor overload current limit relative to P0305 (rated motor current). Dependency: Limited to maximum inverter current or to 400 % of rated motor current (P0305), whichever is the lower. P0640_max = (min(r0209, 4 * P0305) / P0305) * 100 AttachmentP0640.pdf (596 Downloads) |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on