11/23/2023 4:18 PM | |
Joined: 12/13/2005 Last visit: 12/9/2024 Posts: 64 Rating: (3) |
Same problem by me. 1. But I could do for example this: {T,@HH'u'mm'm'ss.SSS's'} But as soon as I use {T....} the IO-Field always shows all the zero values: so 15sec becomes 00u00m15.000s . I would like to see just 15.000s Anyone an idea? 2. As soon I use {T....} and then in runtime I click on the IO-Field I get a popup to input HH,MM,SS AM/PM Without something in the output format. I get a popup to input DD,HH,MM,SS.SSS I prefer this last popup. But How can I force this even if I use the output format? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/24/2023 11:20:24New subject after splitting Last edited by: The Helping Hand at: 11/24/2023 11:21:36Quote from previous Topic added |
|
11/24/2023 11:50 AM | |
Joined: 1/21/2013 Last visit: 1/24/2025 Posts: 3462 Rating: (543)
|
Hi Mr. Q-Bridge, Unfortunately, I could not follow your or Venomz's description, so please describe it in more detail. You can also install the latest image version (now V19) and test it there. I know there was a problem with the time format in the past, but since I cannot follow your description, it is up to you to test it with the current version. Kind regards |
Follow us on