10/21/2012 11:36 AM | |
Posts: 3 Rating: (0) |
Dear all I have a project with a CPU 315-2DP, IM153-2, CP343-1 and 2 ET-200M and 2 AI card(331-7KF02-0AB0)and 2 AO card (332-5HD01-0AB0) I need to be IO redundancy.In fact I have an analog input signal and analog output signal and if the AI card in first rack fail, another card in second rack check the redundancy . Somebody pls check my attach file and complete io redaundancy project . thanks very much AttachmentIO_RED_HELP.zip (71 Downloads) |
Last edited by: saman_he at: 10/21/2012 11:40 AMLast edited by: saman_he at: 10/21/2012 11:39 AMi added attach file |
|
10/21/2012 2:30 PM | |
Joined: 10/7/2005 Last visit: 9/9/2024 Posts: 3019 Rating: (1054)
|
Hello saman_he as you project is empty (apart from HWconfig) my question to you is this: Would you really trust someone that you don't know and have never met to develop software for you that you are ultimately responsible for? If the answer is "Yes", I suggest you place it on www.freelancer.com.au or similar outsourcing site and at least pay someone to do your work for you. Before you do so though, I'd advice you toditch your S7-300 and go for an S7-400H solution which - in my humble oponion - isthe only sensible Siemens choice if I/O redundancy is required. Should the answer be "No" though, I'd still advice you to ditch your S7-300 and go for an S7-400H solution, study the manuals, have a go at developing the software yourself and revert back here for any specific problemsor questions you may encounter along the way. I hope this helps |
Last edited by: fritz at: 10/21/2012 2:34 PMCheers |
|
This contribution was helpful to1 thankful Users |
10/21/2012 3:04 PM | |
Posts: 3 Rating: (0) |
Dear friend , fritz thank you for your support and your answer but i use as SFC13 and OB82 in my project but i can not use as SFC13 really i can not find how to use SFC13 in project in manual project ay siemens in OB82 write STL and i can not undrestand how to work and can not change to FBD i attach OB82 in project and please guide me to change to FBD thanks for you support again sam AttachmentIO_RED_HELP1.zip (60 Downloads) |
Follow us on