11/10/2021 12:31 AM | |
Joined: 9/3/2019 Last visit: 11/12/2021 Posts: 2 Rating:
|
Hello experts I'm new in both Linux and mPCIe cards. My hardware: IOT2050 Basic with the latest image version provided by you and a Sierra MC7700. I cannot find I way to make it work with the IOT2050. I've done research in the forum an make some tests but nothing seems to work. I've followed the pdf provided here by bergmanu https://support.industry.siemens.com/tf/ww/en/posts/how-to-use-mpcie-umts-lte-card/251844 I know the card used in the pdf is different and based on this statement taken from the forum "We do have some sierra drivers integrated, but we are unsure if this model requires any additional kernel configuration." I'm aware that the card might or might not work as easy as other models/brands. From the tests I've been doing I've gotten the following outputs: The last step of the pdf:
Output of mmcli -m 0 (In the Status column > state stays at "connecting"):
Output of dmesg | grep usb:
Output of usb-devices:
I can even send AT commands with Minicom through ttyUSB2, however I'm not able to change the state to "connected". Thank you in advance. |
Last edited by: JohnNawi04 at: 11/10/2021 00:33:17 |
|
Follow us on