4/19/2022 4:21 PM | |
Joined: 12/17/2021 Last visit: 4/27/2022 Posts: 11 Rating:
|
Hi, this is an IOT2050 advanced. The USB key could boot on other IOT2050. But we can't boot on it because we haven't changed the boot order. This is the first start of the IOT. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/20/2022 09:52:48New subject after splitting |
|
4/25/2022 5:06 PM | |
Joined: 4/28/2015 Last visit: 11/28/2023 Posts: 3287 Rating:
|
Hi, you need to use the Example Image V1.2.2 and flash it to a SD card and boot the IOT2050 from this SD card. The internal eMMc is empty with FS:04 (due to the fact that no IndOS is yet available). You can then either run the IOT2050 from the SD card or follow the process described here to flash this Example Image to the internal eMMc. Best regards! |
4/27/2022 12:36 PM | |
Joined: 4/28/2015 Last visit: 11/22/2023 Posts: 570 Rating:
|
You need to quote the value you want to assign to the variable now. That's a subtle change in the new fw_setenv tool we inherited while moving to Debian 11. See also https://groups.google.com/g/swupdate/c/waS74gmIy6M/m/zFf53vnnBAAJ |
Follow us on