10/24/2016 5:20 PM | |
Joined: 9/27/2006 Last visit: 6/8/2023 Posts: 12037 Rating:
|
Hello Grey; The Bus module 6ES7 1895-7HA00-0XA0 is compatible with one P.S. module and one IM 153-2; the -7HB Bus module is designed to hold 2 x 400mm-wide I/O modules. ET200M, BUS UNIT F. P.S. AND IM-153-2 ET200M, BUS UNIT F. 2 40MM I/O MODULES For a redundant IM-153-2 setup, you would need this model of Bus module: https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/6ES7195-7HD10-0XA0 Verify the compatibility of your version of bus unit and IM 153-2, see this FAQ: Which bus modules can you use with the interface modules of the ET 200M? https://support.industry.siemens.com/cs/fr/en/view/109479504 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/24/2016 5:21:24 PMLast edited by: dchartier at: 10/24/2016 6:46:03 PM |
|
Follow us on