8/23/2021 11:11 AM | |
Joined: 9/19/2017 Last visit: 4/5/2023 Posts: 6 Rating:
|
I have a question: In TIA 16, when you want to "open a face plate in a pop-up" from a faceplate, the Tag Interface of the (base) faceplate had to be equal to the pop-up faceplate. What causes me to have Tags connected to the pop-up faceplate I dont need in that faceplate (I understand that the base faceplate needs all tags, of course) As I see that there have been changes to the functions options in TIA 17, so I was wondering: Is it now possible to assign a tag/tags (they are all UDT Tags) to a call "opening a faceplate in a pop-up" from a faceplate? (like you can assign a tag when opening a faceplate in a pop-up from the screens) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/07/2021 14:19:38New subject after splitting |
|
8/28/2021 2:34 PM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
Hi, TIP: Property interface of type configuration script can’t be linked directly to some properties like Text Box, Text. However it could be done indirectly by scripting, e.g. by loading the Faceplate event. Example:
Sample project AttachmentReadConfigurationString_20210828_0928.zip (749 Downloads) |
Denilson Pegaia |
|
1/26/2024 2:15 PM | |
Joined: 3/13/2015 Last visit: 3/8/2025 Posts: 9 Rating:
|
Hello LauraW You will find the solution in this document Attachment109812366_Unified_FaceplatesTT_en_V10.pdf (423 Downloads) |
Last edited by: Jen_Moderator at: 01/29/2024 09:29:14PDF attached from link. Uğur Öz |
|
Follow us on