Industry Online Support
Technical Forum
7/18/2011 11:34 AM | |
Posts: 7 Rating:
|
Thank you... but one doubt....about writing traversing programs....is it possible to create traversing programs only with the software "parameterize FM354" and transfer to CPU in form of SDB. if YES it gives a feel that FM354 only suitable for applications where NC programs are not frequently changed. In our application frequent change of NC programs is required. NOW we can't expect CNC operator to be skilled enough to parameterize FM and donwload to CPU as and when change in NC program is needed. so I just wondered how to create NC program using general OP/MP. so that Operator of machine creates it with ease just like any other CNC machine and without presence of commissioning engineer. thanks in advance Splitted from is it possible to use bigger OPs like MP277 10" as graphical interface between user and FM354. |
Last edited by: O_Moderator at: 7/19/2011 12:28 PMnew subject after splitting |
|
Follow us on