3/1/2020 9:52 AM | |
Joined: 8/4/2019 Last visit: 9/3/2024 Posts: 15 Rating: (0) |
Dear Experts, Is it possible to run S120 book let thorough terminal with out any plc ?, I have connected and programed(with your help) as basic inputs like fixed speed and and jog parameters . My hardware configuration is : Cu -320:6SL3040-0MA00-0AA1,Single motor module:6SL3120-1TE13-0AA0, Basic line module -6SL3130-1TE220AA0 , CF Card 6SL305-0CG00-1AA0 If I can run please the specify important parameters. Please advice me . Regards, Sudhy ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/02/2020 06:56:58New subject after splitting |
|
3/1/2020 12:05 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Sinamics S120 drives are high performance frequency converters and mostly application involves in networking & achieving complex task. Its not worthy to adopt those drives control via terminals only & for single motor application. For the single motor specific application, user has choice of G & V series converters which can be adopt for specific application. BTW you can refer SINAMICS S120 Getting Started with the STARTER Commissioning Tool application example which will help you to understand S120 commissioning. HTH |
Last edited by: PISCEAN 2010 at: 03/01/2020 12:06:46Last edited by: Jen_Moderator at: 03/02/2020 06:59:53Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on