5/4/2021 9:10 PM | |
Posts: 6 Rating:
|
Hello DJ_1, I see that this thread is old but, anyway I would like to as a question. Is it possible to set up Login/Password to access MiniWeb or Sm@art server without being present in front of HMI? Is it possible to do it from TIA Portal? My problem is that the machine I am working on is already installed and working in a very remote location. I do not want the client or local people to go into HMI settings to set up "User Administration". But I have a PC inside the electrical panel with TIA Portal 15.1 on it and connected to HMI and PLC. I have remote access to that PC. I have already activated MiniWeb and Sm@artServer in TIA Portal and loaded the project to HMI. When I am trying to access MiniWeb or Sm@artServer I am asked to enter Login/Password. I have read in some manuals that I need to go to HMI settings "the WInCC Internet Settings -> "Webserver" -> User Administration (HMI control panel)" I hope that there should be a way to do it completely remotely, from TIA Portal on a locally connected PC. I would very much appreciate any help with this subject! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/05/2021 09:19:45New subject after splitting |
|
5/5/2021 9:25 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject Create password for Miniweb/HTML pages from TIA Portal is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
Follow us on