8/12/2021 6:10 PM | |
Joined: 1/16/2015 Last visit: 3/20/2025 Posts: 11 Rating:
|
Hi, do you happen to konw if it is also possible to use the S7-PLCSIM (CPU 300) in conjunction with a simulatated WinCC Unified? I gave it a try, but no success. PG / PC & netwerk settings are fine. Wouter ------------------------------------------------------------------------------------------ |
Last edited by: WouterKUL at: 08/12/2021 18:11:04Last edited by: Jen_Moderator at: 08/13/2021 09:04:35New subject after splitting |
|
8/13/2021 1:49 PM | |
Joined: 6/22/2017 Last visit: 4/16/2025 Posts: 421 Rating:
|
I can confirm, it only worked with the S7-1500 PLCSIM for me. |
4/5/2022 12:21 PM | |
Joined: 9/23/2005 Last visit: 4/21/2025 Posts: 4406 Rating:
|
Hi, In TIA V16:
In TIA V17:
Here there is attached a sample program with S7-1200 and WinCC Unified that run with PLCSim. AttachmentProject4_20220405_0715.zip (1029 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
Follow us on