2/11/2019 3:14 PM | |
Joined: 10/30/2018 Last visit: 7/7/2022 Posts: 63 Rating:
|
Hi again, our designer has made a little change in the planning and we are no more using the 16/17 pins for the enable/Stop . instead they wish to use the safety feature with the Inverter. is it possible to use the safety (stop) with CU310PN from the software and does that mean i would need to put an additional safety telegramm ? thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/12/2019 11:00:37 AMNew subject after splitting |
|
2/12/2019 3:36 PM | |
Joined: 10/11/2006 Last visit: 2/6/2023 Posts: 5417 Rating:
|
Hello, you can use safety integrated functions via digital inputs of the CU310-2 or via PROFIsafe telegram of a F-PLC. |
With best regards, |
|
Follow us on