9/14/2010 4:36 PM | |
Posts: 20 Rating: (0) |
I have another question. The profisafe message frame lengthis 3 bytes (words). Is it true that the first byte (word) can by used to send and receivedata between CU310PN and the PLC? The other two bytes (2 and 3) are been used by the profisafe protocol. For additionaldata you have to use the standard message frame.Is this correct ? Thankyou. Splitted from sinamics s120 cu310 PN Profisafe. |
Last edited by: O_Moderator at: 9/16/2010 8:10 AMnew subject after splitting Last edited by: elmucho at: 9/15/2010 1:45 PM |
|
Follow us on