Industry Online Support
Technical Forum
8/19/2010 3:43 PM | |
Posts: 5 Rating: (0) |
Would appreciate if experts could advice me on this subject. |
8/19/2010 4:08 PM | |
Joined: 9/27/2006 Last visit: 1/22/2025 Posts: 12330 Rating: (2702) |
Hello Gan; As far as electronic records/signature maintenance and GAMP procedures, PLCs are not often the source of the compliance software. This is generally done in HMI/SCADA programs that comply with CFR part 11. Wonderware and Rockwellfor example have add-on programs for their softwares to add compliance to their automation systems. Siemens does the same for WinCC Flexible HMIs (specific models are presentedon the FAQ)and PC-based runtime: http://support.automation.siemens.com/WW/view/en/24327008 and it is built-in the Simatic Batch add-on for WinCC: https://www.automation.siemens.com/mcms/human-machine-interface/en/visualization-software/scada/wincc-options/simatic-batch-for-wincc/Pages/Default.aspx?HTTPS=REDIR Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/19/2010 8:55 PM |
|
This contribution was helpful to1 thankful Users |
8/21/2010 2:45 AM | |
Posts: 5 Rating: (0) |
Thanks for the advice |
Follow us on