10/23/2020 10:12 PM | |
Joined: 7/8/2018 Last visit: 2/13/2021 Posts: 1 Rating:
|
Is same type of PLCSim included in both STEP 7 Basic and STEP 7 Professional licenses? In other words, if someone buys STEP 7 Basic (TIA Portal), then would the PLCSim included in it could be used to simulate S7-1500 and ET 200SP as well, although STEP 7 Basic license can be used to program S7-1200 only? In the picture shown, the STEP7 Basic DVD package includes the DVD which is stated as "PLCSIM" only but it is not clear if it is meant for S7-1200 only or S7-1200/S7-1500/ET 200SP/S7-300/S7-400 can also be used just as PLCSim included with STEP 7 Professional. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2020 09:41:19New subject after splitting |
|
10/24/2020 7:58 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi Autogen, Look page 10 and 11 Operating and Programming plcsim v16 With best regards H |
Last edited by: Jen_Moderator at: 10/26/2020 09:43:09Optimized link. "Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
This contribution was helpful to
1 thankful Users |
Follow us on