10/26/2020 8:23 AM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
hello I want an alarm to be generated when the MOTOR is started and an alarm to be generated when the MOTOR is turned off(I WANT USE FEEDBACK SIGNAL).I use external messaging OF MOTL BLOCK, there is a problem. It is not recorded accurately or only one is recorded. Is there a problem if these inputs(EXTMSG1-2-3) change status at the same time? ------------------------------------------------------------------------------------------ |
Last edited by: PLC2011 at: 10/26/2020 08:26:59Last edited by: Jen_Moderator at: 10/26/2020 11:58:06New subject after splitting |
|