3/13/2019 6:24 PM | |
Joined: 1/10/2019 Last visit: 4/30/2021 Posts: 8 Rating:
|
Is there a way to avoid scanning and enter the PLC IP address somewhere? thank you Loris ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/14/2019 10:56:12 AMNew subject after splitting |
|
3/20/2019 1:30 PM | |
Joined: 8/3/2009 Last visit: 3/24/2025 Posts: 15056 Rating:
|
Hello xLoris ?? can you please explain your usecase or write a more detailed question? Which Versions do you use? which Network structure do you use? ... Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/23/2019 9:00 AM | |
Joined: 1/10/2019 Last visit: 4/30/2021 Posts: 8 Rating:
|
Hi Murof, my questions are meaningless because your should read the original thread. The current thread has been splitted by the moderator from previous topic "VPN : PLC scan not working ?" https://support.industry.siemens.com/tf/ww/en/posts/197287/ The issue is: in case the "Search device.." does not work, can I connect to a PLC by telling TIA to connect to my devices' IP address , for example 192.168.0.222 ? thanks, Loris |
Last edited by: xLoris at: 3/23/2019 9:00:51 AM |
|
3/23/2019 3:28 PM | |
Posts: 2826 Rating:
|
Connecting to the PLC without search should be possible. See if the attachment bring you closer. |
This contribution was helpful to
2 thankful Users |
Follow us on