7/28/2021 3:43 PM | |
Joined: 5/16/2018 Last visit: 7/29/2022 Posts: 3 Rating:
|
Is there a way to re-run the initial setup from ssh? e.g. change the network interface settings ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/29/2021 08:35:12New subject after splitting |
|
7/28/2021 4:23 PM | |
Joined: 4/28/2015 Last visit: 12/8/2023 Posts: 3298 Rating:
|
Hi, yes, just log in and call
Best regards! |
This contribution was helpful to
1 thankful Users |
7/29/2021 2:10 PM | |
Joined: 4/28/2015 Last visit: 12/8/2023 Posts: 3298 Rating:
|
Hi, there is a documentation from Mentor available, it is attached. You can start in chapter 4, the prior ones are not relevant. Chapter 4 is almost the same as chapter 1 in my documentation, in chapter 5 there are some additional topics mentioned. Best regards! Attachmentindustrial_os_iot2050_gs_V2.1.pdf (183 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on