6/27/2018 10:35 AM | |
Joined: 10/29/2014 Last visit: 2/1/2023 Posts: 2 Rating:
|
Hello everyone, It would be greatly appreciated if I get some help or an explanation at least for the problem I have. I am using TIA portal V15 Update 2, and after using for a while I keep getting the message: Consumption of application resources (0024:000004) Consumption of application resources has almost reached a critical limit. You should consider closing some of the opened editors before opening any new ones. You will not be able to open any additional editors when the critical limit for the consumption of the application resources is reached. I am using Windows 10 latest version, I have 32GB of RAM and TIA portal is installed on an SSD (check the picture of system resources) Is there any way to increase the application allocated resources ? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/28/2018 7:35:54 AMNew subject after splitting |
|
6/28/2018 11:20 PM | |
Posts: 1 Rating:
|
SAME ISSUE HERE SIEMENS - IS THERE A FIX? |
6/29/2018 4:41 AM | |
Joined: 12/18/2014 Last visit: 4/20/2025 Posts: 35140 Rating:
|
If you want an answer from Siemens, then make a Support Request. |
Follow us on