12/16/2020 1:58 PM | |
Joined: 7/25/2017 Last visit: 3/22/2023 Posts: 6 Rating: (0) |
Hello, 2. Is one power supply module(6SL3130-6TE21-6AA4) enough? To provide the power of the following list: 1. 6SL3040-1MA01-0AA0 s120 CU320-2pn 2. 6SL3040-1MA01-0AA0 s120 CU320-2pn 3. 6SL3120-2TE13-0AD0 Double Motor Module; 3,00 A; 1,6 kW 4. 6SL3120-2TE15-0AD0 Double Motor Module; 5,00 A; 2,7 kW 5. 6SL3120-2TE15-0AD0 Double Motor Module; 5,00 A; 2,7 kW 6. 6SL3120-2TE21-0AD0 Double Motor Module; 9,00 A; 9,7 kW 3. The question is about the configuration, will everything be fine if you use one power supply unit for two s120 CU320-2pn? B est regards
|
12/16/2020 2:27 PM | |
Joined: 9/23/2005 Last visit: 10/16/2024 Posts: 4757 Rating: (726) |
Are you asking if it is applicable to have single LM nad two CUs? Yes. |
Regards, |
|
Follow us on