Industry Online Support
Technical Forum
6/18/2013 4:48 AM | |
Posts: 1 Rating: (0) |
I am not sure if there is any barcode generator device in siemens automation products. But I have experience of creating barcode. I was wondering what kind of barcode or barcode generator the customer is asking for. You know, there are different kinds of barcode and barcode generators. So first you should figure out this. Second, you may try to use some other barcode generators which may finish this job. Just make full use of Google. You can find many barcode generators, like Java Class barcode generator, VB.NET barcode generator in WinFroms, etc. Then choose a suitable one. |
6/26/2013 11:53 AM | |
Posts: 2 Rating: (0) |
thanks for sharing, the barcode generators you recommended are really helpful for me. |
This contribution was helpful to1 thankful Users |
6/25/2014 5:26 AM | |
Posts: 1 Rating: (0) |
when we want to deal with barcode, we need two things, one is .net barcode generator to create barcode and .net barcode reader to identify barcodes items. another thing is barcode driver compatible with the barcode application. |
6/26/2014 10:35 AM | |
Posts: 2 Rating: (0) |
Hi, As for me, I am testing the related iphone barcode generator these days. Do you have any ideas about it? Or any good suggestion? I am totally a green hand on barcode generating field. Any suggestion will be appreciated. Thanks in advance. Best regards, Arron |
6/27/2014 10:37 AM | |
Posts: 3 Rating: (0) |
I am very interested about the barcode generators mentioned by arronlee. You seeme to be very familiar with the barcode things, don't if you can kindly offer me some suggestions on barcode generator support vb.net. |
10/13/2014 5:26 AM | |
Posts: 1 Rating: (0) |
Hi,i used ka barcode generator to create a barcode in vb.net, why i choose it is that it can help me create many kinds of linear and 2D barcodes,so i think it can help you no matter what kind of barcodes you want to generate.You can search it in google to find it,it's easy. |
1/23/2015 8:54 AM | |
Posts: 1 Rating: (0) |
As i know,there is a product of Siemens called Facility Prime which contain barcode function.The Tools tab of it contains the Scan Code Generator used to create QR Codes that can be linked to Facility Prime graphics.I hope my answer can help you more or less. |
Last edited by: allenmsith at: 1/26/2015 2:44 AM |
|
1/27/2015 4:51 AM | |
Posts: 4 Rating: (0) |
Thank you for your post. I will try it later. |
Follow us on